< Back to Case Studies

Birtes Elektromekanik A.Ş

Fibox supported the Turkish panel builder Birtes with 2,000 + customised enclosures for a PV project totaling 200 Megawatts.

birtes-final-solution

Industry

EPC

Location

Türkiye

Business Line

Enclosures & cabinets

About the company

Birtes Elektromekanik A.Ş. is a family-owned Turkish company founded in 2020. Leveraging the founders’ 25 years of industry experience, Birtes provides engineering solutions for industrial companies with electrical enclosures, connection systems, electrical components, cable entry systems and consumables.  

Birtes partners with leading European manufacturers to import electrical enclosures and components to the Turkish market. Since 2021, Birtes has been the main partner of Fibox in Türkiye.

Challenges

As solar energy projects grow in scale, the requirements for system reliability, durability, and efficient installation become more demanding.

In a large photovoltaic project in Türkiye, Birtes was responsible for delivering DC combiner box solutions to support a 200 megawatt solar installation. 

The project presented several technical and operational challenges:

  • Ensuring protection in harsh outdoor conditions, including high UV exposure and weather stress.

  • Meeting strict technical requirements such as IP65+ -rated protection and suitability for 1500 V DC installation.

  • Enabling customization of enclosures to fit specific end-customer design requirements. 

  • Managing tight delivery timelines for a large-scale project

  • Supporting integration into DC combiner boxes used to connect photovoltaic strings to inverters 

Our Solutions

Customised modular enclosure design

Fibox provided modular enclosure solutions that could be adapted to Birtes’ specific needs. The design allowed Birtes to modify the enclosure structure to match customer requirements. The solution is based on 2,000 EKUN 180 T and EKTH 130 T enclosures with EKTZR accessories to meet the needs of the project. 

birtes-solar-project-close-upx300x225 (1)

Engineered for demanding conditions

The enclosures were designed to withstand outdoor environments, including strong UV exposure and varying weather conditions. They also met required voltage and protection standards for solar applications.

airview-of-solar-plan-in-turkey (1)

Reliable delivery and support

Fibox delivered 2,000 customized enclosures in bulk, supporting efficient logistics and cost management. Continuous support during the project ensured that requirements were met and delivery timelines maintained 

close-up-solar-panel-small (1)

Key figures

200 MW

solar project 

2000

Customised modular enclosures

 

IP 66

standard

There were no problems at all. Fibox understood the requirements of the project fast and were very direct on delivery times.

Murat Aseleten

founder of Birtes Elektromekanik A.Ş.

birtes-final-solution
Fibox was helpful and supportive throughout the project and did everything they could to support us and our customers.

Murat Aseleten

founder of Birtes Elektromekanik A.Ş.

birtes-final-solution
I was sure that if some problems occurred, Fibox would solve them.

Murat Aseleten

founder of Birtes Elektromekanik A.Ş.

birtes-final-solution

Key takeaways

200 MW solar project successfully delivered using Fibox enclosure solutions

For Birtes, this project was not only a successful one – it was a highly impactful project as it presents a big reference for the domestic market and foreign markets. Birtes is now using Fibox enclosures in combination with their engineering services also in the Netherlands and Germany.

2,000 customised enclosures supplied to meet project-specific requirements

Fibox delivered 2,000 EKUN 180 T and EKTH 130 T enclosures with EKTZR accessories to meet the needs of the project. The EK enclosures are designed to withstand harsh environmental conditions and UV exposure which make them excellent for this solar project.

Flexible modular design enabled customer-specific adaptations

The modular design of Fibox’s enclosures allowed Birtes freedom in their own design, while matching the Birtes’s customer requirements.

Reliable delivery and ongoing support ensured smooth project execution

During the project, Birtes worked in close collaboration with Fibox across sales, marketing, customer service, and logistics teams. Birtes, their customer and the end user were all highly satisfied with the product quality and service from Fibox.

Products used in Birtes project

Fibox offers a wide range of durable enclosure and cabinet solutions for extreme weather conditions. In this particular solar project, Birtes used products from EK range. The standard products were customised to suit project specific needs.


                                    EKUN 180 T <br>
                                    2538185
Enclosures

EKUN 180 T
2538185

560 x 380 x 180

Enclosure, PC
Transparent cover


                                    EKTH 130 T <br>
                                    2538167
Enclosures

EKTH 130 T
2538167

560 x 280 x 130

Enclosure, PC
Transparent cover


                                    EKTZR <br>
                                    3730142
Enclosures

EKTZR
3730142

560 x 280 x 50

Extension frame, for enclosures:
560x280x130